Hi Team,
I have two questions.
---------
[Q1]
I understand that “It is necessary that the attenuation (kR) of the two divider networks be equivalent for proper PFC operation.”
If the attenuation (kR) of the two divider networks is different, what kind of concern is there?
<For example>
UCC28070 can’t output the target output voltage etc.
---------
[Q2]
If VSENSE KR is 0.0078(23.5k/(2990k+23.5k)) and VINAC KR is 0.0086(26k/(2990k+26k)) so the two divider networks is different,
what kind of concern is there?
And, could you please let us know “Difference of permissible KR” if you have any information?
<For example>
OK case: Difference of kR is less than 0.1
NG case: Difference of kR is more than 0.1
---------
Regards,
Hide