Hi Team,
I understand that UCC28070 can operate after VCC is stable.
Could you please let us know if you have other sequence (or concern)?
<For example>
I must wait 1ms after VCC is stable etc.
Regards,
Hide
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Hide,
The UCC28070 starts operating as soon as the UVLO is exceeded on VCC
This causes the SS pin to charge and pwm to increase.
If VCC is not stable then something else is happening in your system and it is best to fix this before starting up the pfc.
That is the only issue that I can see .
Regards
John