This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS56637: 4x 22uF output caps, versus 1x 100uF output cap?

Part Number: TPS56637
Is there any compelling reason to not choose a single 100uF output cap, if you can find one at a convenient size/price, instead of using four 22uF caps of the same type in parallel? Similar question on the input stage (one 47uF input cap versus four 10uF caps...). I’m trying to simplify layout.