I'm operating the PMIC in 4-Phase configuration(single output). The measurements via the I2C registers is listed below. As indicated, most of the current is from BUCK0(2.78A). I was expecting the 4 bucks to share the current load equally.
Should the current be equally shared?
Power State:
========================================
Input: 12.1V
----------------------------------------
PMIC 1 (LP875610) - Connected
[ OK ] Clock
[ OK ] Temperature
[ OK ] Overvoltage
[ OK ] 0: 0.850V, 2.780A
[ OK ] 1: 0.850V, 0.740A
[ OK ] 2: 0.850V, 0.760A
[ OK ] 3: 0.850V, 0.660A