This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63710: Design the DC-DC converter for -1Vout , -2A Iout

Part Number: TPS63710
Other Parts Discussed in Thread: TPS54424

I have requirement of DC-DC inverting buck converter which input is 5V(Vin) and Output voltage -1V (Vout) and output sink current of -2A ( Isink ).I got a similar product from Ti Website , the device is TPS63710. Which Iout is -1A. My plan is to connect two TPS63710 device in parallel to achieve the the -2A current.Could someone can confirm on the same whether I can able to meet the requirement .