This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC39002: how to set the master and second

Part Number: UCC39002
Other Parts Discussed in Thread: UCC28950,

Hello john 

The method you mentioned below is as follows. How do I set it up, can you provide the circuit?

Set one up as the master using the voltage amplifier with feedback components.

You set the second amplifier as a voltage follower and feed the comp output of the master into it.

Other question

if the master have issue,one of the other parallel devices will be auto change to master?

  • Hello ,

    The confusion here is caused by a response to your previous question.
    This response referred to the UCC28950 and recommended setting up a master /slave control.
    For details on this please refer to the UCC28950 data sheet

    The UCC39002 does not have a master/slave control relationship.

    Regards

    John