This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM74610-Q1: switching power off with mechanical switch to circuit

Part Number: LM74610-Q1

There is an external N-channel Mosfet that the LM74610 is able to turn OFF and ON based if the polarity is correct of the input battery.  However I want to be able to turn the power OFF to the circuit even if the polarity is correct when I don't want power anymore going to my circuit.  I want to use a mechanical switch to do so.  I DON'T want to put the mechanical switch in line with VIN (battery input).   can I place a SPDT switch between the gate drive(pin 6) of the LM74610 to the external N Channel Mosfet?  When I want the power to go OFF, the mechanical switch would ground the gate of the external N Channel Mosfet and when I want power to turn ON,  I could turn the switch to the ON position which will then allow the gate drive(pin 6) of the LM74610 to drive the gate of the external N Channel mosfet.  Do you see any problem with this method or have any suggestions?  Remember I don't want to put the switch in line with VIN where the battery power comes from