While running evaluation of the bq25601 EVM an unexpected SYS output is observed. In this test, there is no source connected to VBUS, but a charged battery is connected to VBAT.
With a 10 ohm resistor load connected SYS, the proper battery voltage is observed at the SYS pin. If the BATFET is disabled, SYS voltage drops to 0V as expected.
However, with an active load consisting of a switching boost converter connected to SYS and set to output 5V, the response is different. When the charger BATFET is disabled, the SYS voltage drops to about 1V, and output of the boost is still 5V. If a 10 ohm resistor is placed between SYS and ground, the SYS voltage drops to 0V. But if the resistor is removed, SYS voltage returns to 1V. If the 10 ohm resistor is placed on the output of the boost, the SYS voltage remains at 1V (with BATFET disabled).
If the boost converter is disabled and then the BATFET is disabled, the SYS voltage is 1.3V. Boost converter is designed to isolate its input from the output when disabled.
Any ideas why disabling the BATFET does not completely turn off the load?