Hi Team,
WEBENCH Designer for the LM5140-Q1 supports equal or less than 10A.
My customer is considering to use the LM5140-Q1 for the following application.
- VIN: 24V (13V ~ 32V)
- Vout1: 12V
- Iout1: 14.5A
- Vout2: 5V
- Iout2: 14.5A
Can the LM5140-Q1 supports the above application?
Are there any concerns about the LM5140-Q1 application for that?
Could you create the reference application circuit of LM5140-Q1 for that?
Thank you.
Best Regards,
Koshi Ninomiya