This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS759: 10A output

Part Number: TPS759
Other Parts Discussed in Thread: TPS7A85

Hi team,

TPS759 has max 7.5A output, do we have solution to achieve 10A? Like paralle two LDO? Thanks.

  • Hi Jeff,

    We have the following reference design which can be used to force sharing between LDO's. This takes advantage of the fact that the TPS7A85 has an NR/SS pin which is the internal reference. Tying these together forces them to share the same reference. This concept could be extrapolating to used 3 devices to get more current. 

    Let me know what you think.