Dear Team,
Could we have your suggestion about 5Vin @300mA LDO with 90dB PSRR?
I found TPS7A20 is the close one. But still not good enough for customer's application.
Ben
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ben,
At what frequency, drop-out, and frequency is the 90dB PSRR required?
Here is a plot showing the PSRR showing different drop-out voltages with V
at 2.8V:
Can you clarify? Also, do you see other devices that have high PSRR? Last but not least is it PSRR or noise that they are concerned with? What is the application and load bring powered?
Thank you,
Hi JCHK,
Vin=3.8V, Vout=3.3V, I_load=400mA
200Hz~200kHz have to close to 90dB.
It's and RF application. Customer design with ADM7154 now.
Ben
Got it, thanks~