This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC27201: external bootstrap diode

Part Number: UCC27201

Hello,
customer wants to drive high gate charge mosfets (approx. >150nC) with switching freq. of 70KHz. Can he drive it with UCC27201 or does he need an external diode to improve drive capability.

Regards, Holger

  • Hello Holger,

    Thank you for supporting the UCC27201. There are a couple of considerations for driving high charge MOSFETs regarding the boot diode.

    I would 1st confirm the average boot diode current required for driving the high side MOSFET. I will assume there is a single 150nC MOSFET, the current required will be the gate charge x fsw or 150nC x 70kHz = 10.5mA. This is well below the internal boot diode average current capability of 100mA.

    I would confirm the boot capacitance required: A simple target is allowing 1V drop for charging the MOSFETs Qg, Cboot = Qg/delta HB or 150nC/1V or 150nF. We recommend oversizing the boot cap for tolerance due to temp and voltage, so a 220nF to 330nF capacitor will be adequate.

    It looks like this application will be OK with the driver internal boot diode.

    Regards,

  • Hello Richard,

    thanks for explanation.

    Customer worried about the peak currents and the peak current capabilities of the bootstrap diode.

    Regards, Holger