Other Parts Discussed in Thread: BQSTUDIO
When I try to import the Battery Calibration.gg file and write the values it works for the most part, but it's not writing the CC Delta value under the calibration menu.
Here's what's in the file:
"Calibration","Data","CC Gain","1.007","mohm"
"Calibration","Data","CC Delta","1.007","mohm"
I find the lowest value I can write and have it save is 5mohm.
Our design uses a 1mOhm sense resistor.
I am able to calibrate voltage, temperature, CC offset, and Board offset successfully.
Any clue why it's not writing?