This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5562: The error about firmware load

Part Number: LP5562


Hi,

I use the following cmds on Linux to use LP5562 LED:

/bin/echo 0 > /sys/bus/i2c/devices/0-0032/run_engine
/bin/echo 3 > /sys/bus/i2c/devices/0-0032/select_engine
/bin/echo "RGB" > /sys/bus/i2c/devices/0-0032/engine_mux
/bin/echo 1 > /sys/bus/i2c/devices/0-0032/firmware/lp5562/loading
/bin/echo "4063D00000000000" > /sys/bus/i2c/devices/0-0032/firmware/lp5562/data
/bin/echo 0 > /sys/bus/i2c/devices/0-0032/firmware/lp5562/loading
/bin/echo 1 > /sys/class/i2c-dev/i2c-0/device/0-0032/run_engine

Although it can work, I find after using "echo 3 > /sys/bus/i2c/devices/0-0032/select_engine" cmd, it has error:
[ 4281.157687] lp5562 0-0032: Direct firmware load for lp5562 failed with error -2
[ 4281.164988] lp5562 0-0032: Falling back to user helper

Is it normal? If not, how do I fix it?

Thanks

Marten

  • Hi Marten,

    Could you share the source driver code?

  • Hi Hardy,

    Sure, please see it in the following:

    /*
     * LP5562 LED driver
     *
     * Copyright (C) 2013 Texas Instruments
     *
     * Author: Milo(Woogyom) Kim <milo.kim@ti.com>
     *
     * This program is free software; you can redistribute it and/or modify
     * it under the terms of the GNU General Public License version 2 as
     * published by the Free Software Foundation.
     */
    
    #include <linux/delay.h>
    #include <linux/firmware.h>
    #include <linux/i2c.h>
    #include <linux/leds.h>
    #include <linux/module.h>
    #include <linux/mutex.h>
    #include <linux/of.h>
    #include <linux/platform_data/leds-lp55xx.h>
    #include <linux/slab.h>
    
    #include "leds-lp55xx-common.h"
    
    #define LP5562_PROGRAM_LENGTH		32
    #define LP5562_MAX_LEDS			4
    
    /* ENABLE Register 00h */
    #define LP5562_REG_ENABLE		0x00
    #define LP5562_EXEC_ENG1_M		0x30
    #define LP5562_EXEC_ENG2_M		0x0C
    #define LP5562_EXEC_ENG3_M		0x03
    #define LP5562_EXEC_M			0x3F
    #define LP5562_MASTER_ENABLE		0x40	/* Chip master enable */
    #define LP5562_LOGARITHMIC_PWM		0x80	/* Logarithmic PWM adjustment */
    #define LP5562_EXEC_RUN			0x2A
    #define LP5562_ENABLE_DEFAULT	\
    	(LP5562_MASTER_ENABLE | LP5562_LOGARITHMIC_PWM)
    #define LP5562_ENABLE_RUN_PROGRAM	\
    	(LP5562_ENABLE_DEFAULT | LP5562_EXEC_RUN)
    
    /* OPMODE Register 01h */
    #define LP5562_REG_OP_MODE		0x01
    #define LP5562_MODE_ENG1_M		0x30
    #define LP5562_MODE_ENG2_M		0x0C
    #define LP5562_MODE_ENG3_M		0x03
    #define LP5562_LOAD_ENG1		0x10
    #define LP5562_LOAD_ENG2		0x04
    #define LP5562_LOAD_ENG3		0x01
    #define LP5562_RUN_ENG1			0x20
    #define LP5562_RUN_ENG2			0x08
    #define LP5562_RUN_ENG3			0x02
    #define LP5562_ENG1_IS_LOADING(mode)	\
    	((mode & LP5562_MODE_ENG1_M) == LP5562_LOAD_ENG1)
    #define LP5562_ENG2_IS_LOADING(mode)	\
    	((mode & LP5562_MODE_ENG2_M) == LP5562_LOAD_ENG2)
    #define LP5562_ENG3_IS_LOADING(mode)	\
    	((mode & LP5562_MODE_ENG3_M) == LP5562_LOAD_ENG3)
    
    /* BRIGHTNESS Registers */
    #define LP5562_REG_R_PWM		0x04
    #define LP5562_REG_G_PWM		0x03
    #define LP5562_REG_B_PWM		0x02
    #define LP5562_REG_W_PWM		0x0E
    
    /* CURRENT Registers */
    #define LP5562_REG_R_CURRENT		0x07
    #define LP5562_REG_G_CURRENT		0x06
    #define LP5562_REG_B_CURRENT		0x05
    #define LP5562_REG_W_CURRENT		0x0F
    
    /* CONFIG Register 08h */
    #define LP5562_REG_CONFIG		0x08
    #define LP5562_PWM_HF			0x40
    #define LP5562_PWRSAVE_EN		0x20
    #define LP5562_CLK_INT			0x01	/* Internal clock */
    #define LP5562_DEFAULT_CFG		(LP5562_PWM_HF | LP5562_PWRSAVE_EN)
    
    /* RESET Register 0Dh */
    #define LP5562_REG_RESET		0x0D
    #define LP5562_RESET			0xFF
    
    /* PROGRAM ENGINE Registers */
    #define LP5562_REG_PROG_MEM_ENG1	0x10
    #define LP5562_REG_PROG_MEM_ENG2	0x30
    #define LP5562_REG_PROG_MEM_ENG3	0x50
    
    /* LEDMAP Register 70h */
    #define LP5562_REG_ENG_SEL		0x70
    #define LP5562_ENG_SEL_PWM		0
    #define LP5562_ENG_FOR_RGB_M		0x3F
    #define LP5562_ENG_SEL_RGB		0x1B	/* R:ENG1, G:ENG2, B:ENG3 */
    #define LP5562_ENG_FOR_W_M		0xC0
    #define LP5562_ENG1_FOR_W		0x40	/* W:ENG1 */
    #define LP5562_ENG2_FOR_W		0x80	/* W:ENG2 */
    #define LP5562_ENG3_FOR_W		0xC0	/* W:ENG3 */
    
    /* Program Commands */
    #define LP5562_CMD_DISABLE		0x00
    #define LP5562_CMD_LOAD			0x15
    #define LP5562_CMD_RUN			0x2A
    #define LP5562_CMD_DIRECT		0x3F
    #define LP5562_PATTERN_OFF		0
    
    static inline void lp5562_wait_opmode_done(void)
    {
    	/* operation mode change needs to be longer than 153 us */
    	usleep_range(200, 300);
    }
    
    static inline void lp5562_wait_enable_done(void)
    {
    	/* it takes more 488 us to update ENABLE register */
    	usleep_range(500, 600);
    }
    
    static void lp5562_set_led_current(struct lp55xx_led *led, u8 led_current)
    {
    	static const u8 addr[] = {
    		LP5562_REG_R_CURRENT,
    		LP5562_REG_G_CURRENT,
    		LP5562_REG_B_CURRENT,
    		LP5562_REG_W_CURRENT,
    	};
    
    	led->led_current = led_current;
    	lp55xx_write(led->chip, addr[led->chan_nr], led_current);
    }
    
    static void lp5562_load_engine(struct lp55xx_chip *chip)
    {
    	enum lp55xx_engine_index idx = chip->engine_idx;
    	static const u8 mask[] = {
    		[LP55XX_ENGINE_1] = LP5562_MODE_ENG1_M,
    		[LP55XX_ENGINE_2] = LP5562_MODE_ENG2_M,
    		[LP55XX_ENGINE_3] = LP5562_MODE_ENG3_M,
    	};
    
    	static const u8 val[] = {
    		[LP55XX_ENGINE_1] = LP5562_LOAD_ENG1,
    		[LP55XX_ENGINE_2] = LP5562_LOAD_ENG2,
    		[LP55XX_ENGINE_3] = LP5562_LOAD_ENG3,
    	};
    
    	lp55xx_update_bits(chip, LP5562_REG_OP_MODE, mask[idx], val[idx]);
    
    	lp5562_wait_opmode_done();
    }
    
    static void lp5562_stop_engine(struct lp55xx_chip *chip)
    {
    	lp55xx_write(chip, LP5562_REG_OP_MODE, LP5562_CMD_DISABLE);
    	lp5562_wait_opmode_done();
    }
    
    static void lp5562_run_engine(struct lp55xx_chip *chip, bool start)
    {
    	int ret;
    	u8 mode;
    	u8 exec;
    
    	/* stop engine */
    	if (!start) {
    		lp55xx_write(chip, LP5562_REG_ENABLE, LP5562_ENABLE_DEFAULT);
    		lp5562_wait_enable_done();
    		lp5562_stop_engine(chip);
    		lp55xx_write(chip, LP5562_REG_ENG_SEL, LP5562_ENG_SEL_PWM);
    		lp55xx_write(chip, LP5562_REG_OP_MODE, LP5562_CMD_DIRECT);
    		lp5562_wait_opmode_done();
    		return;
    	}
    
    	/*
    	 * To run the engine,
    	 * operation mode and enable register should updated at the same time
    	 */
    
    	ret = lp55xx_read(chip, LP5562_REG_OP_MODE, &mode);
    	if (ret)
    		return;
    
    	ret = lp55xx_read(chip, LP5562_REG_ENABLE, &exec);
    	if (ret)
    		return;
    
    	/* change operation mode to RUN only when each engine is loading */
    	if (LP5562_ENG1_IS_LOADING(mode)) {
    		mode = (mode & ~LP5562_MODE_ENG1_M) | LP5562_RUN_ENG1;
    		exec = (exec & ~LP5562_EXEC_ENG1_M) | LP5562_RUN_ENG1;
    	}
    
    	if (LP5562_ENG2_IS_LOADING(mode)) {
    		mode = (mode & ~LP5562_MODE_ENG2_M) | LP5562_RUN_ENG2;
    		exec = (exec & ~LP5562_EXEC_ENG2_M) | LP5562_RUN_ENG2;
    	}
    
    	if (LP5562_ENG3_IS_LOADING(mode)) {
    		mode = (mode & ~LP5562_MODE_ENG3_M) | LP5562_RUN_ENG3;
    		exec = (exec & ~LP5562_EXEC_ENG3_M) | LP5562_RUN_ENG3;
    	}
    
    	lp55xx_write(chip, LP5562_REG_OP_MODE, mode);
    	lp5562_wait_opmode_done();
    
    	lp55xx_update_bits(chip, LP5562_REG_ENABLE, LP5562_EXEC_M, exec);
    	lp5562_wait_enable_done();
    }
    
    static int lp5562_update_firmware(struct lp55xx_chip *chip,
    					const u8 *data, size_t size)
    {
    	enum lp55xx_engine_index idx = chip->engine_idx;
    	u8 pattern[LP5562_PROGRAM_LENGTH] = {0};
    	static const u8 addr[] = {
    		[LP55XX_ENGINE_1] = LP5562_REG_PROG_MEM_ENG1,
    		[LP55XX_ENGINE_2] = LP5562_REG_PROG_MEM_ENG2,
    		[LP55XX_ENGINE_3] = LP5562_REG_PROG_MEM_ENG3,
    	};
    	unsigned cmd;
    	char c[3];
    	int program_size;
    	int nrchars;
    	int offset = 0;
    	int ret;
    	int i;
    
    	/* clear program memory before updating */
    	for (i = 0; i < LP5562_PROGRAM_LENGTH; i++)
    		lp55xx_write(chip, addr[idx] + i, 0);
    
    	i = 0;
    	while ((offset < size - 1) && (i < LP5562_PROGRAM_LENGTH)) {
    		/* separate sscanfs because length is working only for %s */
    		ret = sscanf(data + offset, "%2s%n ", c, &nrchars);
    		if (ret != 1)
    			goto err;
    
    		ret = sscanf(c, "%2x", &cmd);
    		if (ret != 1)
    			goto err;
    
    		pattern[i] = (u8)cmd;
    		offset += nrchars;
    		i++;
    	}
    
    	/* Each instruction is 16bit long. Check that length is even */
    	if (i % 2)
    		goto err;
    
    	program_size = i;
    	for (i = 0; i < program_size; i++)
    		lp55xx_write(chip, addr[idx] + i, pattern[i]);
    
    	return 0;
    
    err:
    	dev_err(&chip->cl->dev, "wrong pattern format\n");
    	return -EINVAL;
    }
    
    static void lp5562_firmware_loaded(struct lp55xx_chip *chip)
    {
    	const struct firmware *fw = chip->fw;
    
    	if (fw->size > LP5562_PROGRAM_LENGTH) {
    		dev_err(&chip->cl->dev, "firmware data size overflow: %zu\n",
    			fw->size);
    		return;
    	}
    
    	/*
    	 * Program memory sequence
    	 *  1) set engine mode to "LOAD"
    	 *  2) write firmware data into program memory
    	 */
    
    	lp5562_load_engine(chip);
    	lp5562_update_firmware(chip, fw->data, fw->size);
    }
    
    static int lp5562_post_init_device(struct lp55xx_chip *chip)
    {
    	int ret;
    	u8 cfg = LP5562_DEFAULT_CFG;
    
    	/* Set all PWMs to direct control mode */
    	ret = lp55xx_write(chip, LP5562_REG_OP_MODE, LP5562_CMD_DIRECT);
    	if (ret)
    		return ret;
    
    	lp5562_wait_opmode_done();
    
    	/* Update configuration for the clock setting */
    	if (!lp55xx_is_extclk_used(chip))
    		cfg |= LP5562_CLK_INT;
    
    	ret = lp55xx_write(chip, LP5562_REG_CONFIG, cfg);
    	if (ret)
    		return ret;
    
    	/* Initialize all channels PWM to zero -> leds off */
    	lp55xx_write(chip, LP5562_REG_R_PWM, 0);
    	lp55xx_write(chip, LP5562_REG_G_PWM, 0);
    	lp55xx_write(chip, LP5562_REG_B_PWM, 0);
    	lp55xx_write(chip, LP5562_REG_W_PWM, 0);
    
    	/* Set LED map as register PWM by default */
    	lp55xx_write(chip, LP5562_REG_ENG_SEL, LP5562_ENG_SEL_PWM);
    
    	return 0;
    }
    
    static int lp5562_led_brightness(struct lp55xx_led *led)
    {
    	struct lp55xx_chip *chip = led->chip;
    	static const u8 addr[] = {
    		LP5562_REG_R_PWM,
    		LP5562_REG_G_PWM,
    		LP5562_REG_B_PWM,
    		LP5562_REG_W_PWM,
    	};
    	int ret;
    
    	mutex_lock(&chip->lock);
    	ret = lp55xx_write(chip, addr[led->chan_nr], led->brightness);
    	mutex_unlock(&chip->lock);
    
    	return ret;
    }
    
    static void lp5562_write_program_memory(struct lp55xx_chip *chip,
    					u8 base, const u8 *rgb, int size)
    {
    	int i;
    
    	if (!rgb || size <= 0)
    		return;
    
    	for (i = 0; i < size; i++)
    		lp55xx_write(chip, base + i, *(rgb + i));
    
    	lp55xx_write(chip, base + i, 0);
    	lp55xx_write(chip, base + i + 1, 0);
    }
    
    /* check the size of program count */
    static inline bool _is_pc_overflow(struct lp55xx_predef_pattern *ptn)
    {
    	return ptn->size_r >= LP5562_PROGRAM_LENGTH ||
    	       ptn->size_g >= LP5562_PROGRAM_LENGTH ||
    	       ptn->size_b >= LP5562_PROGRAM_LENGTH;
    }
    
    static int lp5562_run_predef_led_pattern(struct lp55xx_chip *chip, int mode)
    {
    	struct lp55xx_predef_pattern *ptn;
    	int i;
    
    	if (mode == LP5562_PATTERN_OFF) {
    		lp5562_run_engine(chip, false);
    		return 0;
    	}
    
    	ptn = chip->pdata->patterns + (mode - 1);
    	if (!ptn || _is_pc_overflow(ptn)) {
    		dev_err(&chip->cl->dev, "invalid pattern data\n");
    		return -EINVAL;
    	}
    
    	lp5562_stop_engine(chip);
    
    	/* Set LED map as RGB */
    	lp55xx_write(chip, LP5562_REG_ENG_SEL, LP5562_ENG_SEL_RGB);
    
    	/* Load engines */
    	for (i = LP55XX_ENGINE_1; i <= LP55XX_ENGINE_3; i++) {
    		chip->engine_idx = i;
    		lp5562_load_engine(chip);
    	}
    
    	/* Clear program registers */
    	lp55xx_write(chip, LP5562_REG_PROG_MEM_ENG1, 0);
    	lp55xx_write(chip, LP5562_REG_PROG_MEM_ENG1 + 1, 0);
    	lp55xx_write(chip, LP5562_REG_PROG_MEM_ENG2, 0);
    	lp55xx_write(chip, LP5562_REG_PROG_MEM_ENG2 + 1, 0);
    	lp55xx_write(chip, LP5562_REG_PROG_MEM_ENG3, 0);
    	lp55xx_write(chip, LP5562_REG_PROG_MEM_ENG3 + 1, 0);
    
    	/* Program engines */
    	lp5562_write_program_memory(chip, LP5562_REG_PROG_MEM_ENG1,
    				ptn->r, ptn->size_r);
    	lp5562_write_program_memory(chip, LP5562_REG_PROG_MEM_ENG2,
    				ptn->g, ptn->size_g);
    	lp5562_write_program_memory(chip, LP5562_REG_PROG_MEM_ENG3,
    				ptn->b, ptn->size_b);
    
    	/* Run engines */
    	lp5562_run_engine(chip, true);
    
    	return 0;
    }
    
    static ssize_t lp5562_store_pattern(struct device *dev,
    				struct device_attribute *attr,
    				const char *buf, size_t len)
    {
    	struct lp55xx_led *led = i2c_get_clientdata(to_i2c_client(dev));
    	struct lp55xx_chip *chip = led->chip;
    	struct lp55xx_predef_pattern *ptn = chip->pdata->patterns;
    	int num_patterns = chip->pdata->num_patterns;
    	unsigned long mode;
    	int ret;
    
    	ret = kstrtoul(buf, 0, &mode);
    	if (ret)
    		return ret;
    
    	if (mode > num_patterns || !ptn)
    		return -EINVAL;
    
    	mutex_lock(&chip->lock);
    	ret = lp5562_run_predef_led_pattern(chip, mode);
    	mutex_unlock(&chip->lock);
    
    	if (ret)
    		return ret;
    
    	return len;
    }
    
    static ssize_t lp5562_store_engine_mux(struct device *dev,
    				     struct device_attribute *attr,
    				     const char *buf, size_t len)
    {
    	struct lp55xx_led *led = i2c_get_clientdata(to_i2c_client(dev));
    	struct lp55xx_chip *chip = led->chip;
    	u8 mask;
    	u8 val;
    
    	/* LED map
    	 * R ... Engine 1 (fixed)
    	 * G ... Engine 2 (fixed)
    	 * B ... Engine 3 (fixed)
    	 * W ... Engine 1 or 2 or 3
    	 */
    
    	if (sysfs_streq(buf, "RGB")) {
    		mask = LP5562_ENG_FOR_RGB_M;
    		val = LP5562_ENG_SEL_RGB;
    	} else if (sysfs_streq(buf, "W")) {
    		enum lp55xx_engine_index idx = chip->engine_idx;
    
    		mask = LP5562_ENG_FOR_W_M;
    		switch (idx) {
    		case LP55XX_ENGINE_1:
    			val = LP5562_ENG1_FOR_W;
    			break;
    		case LP55XX_ENGINE_2:
    			val = LP5562_ENG2_FOR_W;
    			break;
    		case LP55XX_ENGINE_3:
    			val = LP5562_ENG3_FOR_W;
    			break;
    		default:
    			return -EINVAL;
    		}
    
    	} else {
    		dev_err(dev, "choose RGB or W\n");
    		return -EINVAL;
    	}
    
    	mutex_lock(&chip->lock);
    	lp55xx_update_bits(chip, LP5562_REG_ENG_SEL, mask, val);
    	mutex_unlock(&chip->lock);
    
    	return len;
    }
    
    static LP55XX_DEV_ATTR_WO(led_pattern, lp5562_store_pattern);
    static LP55XX_DEV_ATTR_WO(engine_mux, lp5562_store_engine_mux);
    
    static struct attribute *lp5562_attributes[] = {
    	&dev_attr_led_pattern.attr,
    	&dev_attr_engine_mux.attr,
    	NULL,
    };
    
    static const struct attribute_group lp5562_group = {
    	.attrs = lp5562_attributes,
    };
    
    /* Chip specific configurations */
    static struct lp55xx_device_config lp5562_cfg = {
    	.max_channel  = LP5562_MAX_LEDS,
    	.reset = {
    		.addr = LP5562_REG_RESET,
    		.val  = LP5562_RESET,
    	},
    	.enable = {
    		.addr = LP5562_REG_ENABLE,
    		.val  = LP5562_ENABLE_DEFAULT,
    	},
    	.post_init_device   = lp5562_post_init_device,
    	.set_led_current    = lp5562_set_led_current,
    	.brightness_fn      = lp5562_led_brightness,
    	.run_engine         = lp5562_run_engine,
    	.firmware_cb        = lp5562_firmware_loaded,
    	.dev_attr_group     = &lp5562_group,
    };
    
    static int lp5562_probe(struct i2c_client *client,
    			const struct i2c_device_id *id)
    {
    	int ret;
    	struct lp55xx_chip *chip;
    	struct lp55xx_led *led;
    	struct lp55xx_platform_data *pdata = dev_get_platdata(&client->dev);
    	struct device_node *np = client->dev.of_node;
    
    	if (!pdata) {
    		if (np) {
    			pdata = lp55xx_of_populate_pdata(&client->dev, np);
    			if (IS_ERR(pdata))
    				return PTR_ERR(pdata);
    		} else {
    			dev_err(&client->dev, "no platform data\n");
    			return -EINVAL;
    		}
    	}
    
    	chip = devm_kzalloc(&client->dev, sizeof(*chip), GFP_KERNEL);
    	if (!chip)
    		return -ENOMEM;
    
    	led = devm_kzalloc(&client->dev,
    			sizeof(*led) * pdata->num_channels, GFP_KERNEL);
    	if (!led)
    		return -ENOMEM;
    
    	chip->cl = client;
    	chip->pdata = pdata;
    	chip->cfg = &lp5562_cfg;
    
    	mutex_init(&chip->lock);
    
    	i2c_set_clientdata(client, led);
    
    	ret = lp55xx_init_device(chip);
    	if (ret)
    		goto err_init;
    
    	ret = lp55xx_register_leds(led, chip);
    	if (ret)
    		goto err_register_leds;
    
    	ret = lp55xx_register_sysfs(chip);
    	if (ret) {
    		dev_err(&client->dev, "registering sysfs failed\n");
    		goto err_register_sysfs;
    	}
    
    	return 0;
    
    err_register_sysfs:
    	lp55xx_unregister_leds(led, chip);
    err_register_leds:
    	lp55xx_deinit_device(chip);
    err_init:
    	return ret;
    }
    
    static int lp5562_remove(struct i2c_client *client)
    {
    	struct lp55xx_led *led = i2c_get_clientdata(client);
    	struct lp55xx_chip *chip = led->chip;
    
    	lp5562_stop_engine(chip);
    
    	lp55xx_unregister_sysfs(chip);
    	lp55xx_unregister_leds(led, chip);
    	lp55xx_deinit_device(chip);
    
    	return 0;
    }
    
    static const struct i2c_device_id lp5562_id[] = {
    	{ "lp5562", 0 },
    	{ }
    };
    MODULE_DEVICE_TABLE(i2c, lp5562_id);
    
    #ifdef CONFIG_OF
    static const struct of_device_id of_lp5562_leds_match[] = {
    	{ .compatible = "ti,lp5562", },
    	{},
    };
    
    MODULE_DEVICE_TABLE(of, of_lp5562_leds_match);
    #endif
    
    static struct i2c_driver lp5562_driver = {
    	.driver = {
    		.name	= "lp5562",
    		.of_match_table = of_match_ptr(of_lp5562_leds_match),
    	},
    	.probe		= lp5562_probe,
    	.remove		= lp5562_remove,
    	.id_table	= lp5562_id,
    };
    
    module_i2c_driver(lp5562_driver);
    
    MODULE_DESCRIPTION("Texas Instruments LP5562 LED Driver");
    MODULE_AUTHOR("Milo Kim");
    MODULE_LICENSE("GPL");
    

    Thanks

    Marten

  • Hi Marten,

    Sorry that we cannot find the original engineer for this code. And we have bare linux knowledge since we are all hardware engineer, the support would be limit.

    I could not find the select_engine in below functions. Is there any missed code?

  • Hi Marten,

    Sorry that we have no Linux test environment and cannot help with it.