Hi Sir,
May I learn from you does TI have a Buck converter or controller solution can support 150W and integrated PD function?
Thank you.
Edward Chen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Edward,
We do not have a buck converter with integrated PD functionality
We use the LM3489 on our TPS65987DEVM which has a bypass mode that allows you to pass through a barrel jack or central supply. You can negotiate a 20V contract with the TPS65987D which will then control the LM3489 to pass through a 20V supply to VBUS.
What application are you designing for where you need a PD controller to source this much power? The cable you use also must be taken into account as the amount of power a PD controller can supply will be limited to the cable capabilites
You can also refer to the Power Duo source board for reference