Other Parts Discussed in Thread: BQSTUDIO, EV2400
Hi,
I am trying to set up BQ28Z610 without using "BQSTUDIO", but there is a place where it is not working.
Can you answer the following questions?
1. Does the RSOC value indicate the remaining capacity in% of the maximum capacity of the battery?
2. For "FD", "FC", "TD", and "TC", use a cell with a voltage of 7200mV. Does the set value match with half of the target value?
3.What is the correct answer for Voltage at EoC for the maximum voltage of 7200mV to charge?
4. TS terminal is not connected. Is it necessary to set internal “TS” in “Temperature Enable” setting?
5. Is it possible to return to the factory settings?
6. I am writing without using "BQSTUDIO" in the attachment settings, but there are problems that the battery cannot be charged and the correct value cannot be read with CellVoltage.
Can you point out the problem?
Hope to hear from you soon!