This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27542-G1: solution ask (v.s. BQ27750)

Part Number: BQ27542-G1
Other Parts Discussed in Thread: BQ27Z561-R1, BQ27742-G1

Hi Team , 

My customer is surveying the gauge solution  and would like to ask which solution (BQ27542-G1 or BQ27750) is better fit for below requirement

1. battery pack side gauge

2. battery cell capacity is about 3700mAH

3. Accuracy Error <=1%

4. compensate for transient effect and aging as well as temperature changing

5. needed able to achieve function to read battery's charge cycling , and battery healthy (like mobile phone's app)

per my check , both solution is fit for point 1.2.5 , BQ27542-G1 looks it can fit point 4 also ,but it didn't shown the battery monitor accuracy percentage in d/s, and for BQ27750, it can fit the accuracy below 1% , but I don't found the description in d/s shown it can support point 4.

please kindly help for the suggestion , thanks!