This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23523: About IEC 62368

Part Number: TPS23523
Other Parts Discussed in Thread: TPS2663,

Hi,

Is this device IEC62368 tested?
Customer is looking for products with the following specifications that support negative voltage.
Is there a recommended efuse that supports IEC62368?

・Vin=-52V
・Output current =2~4A
・IEC62368 support

Regards,
Yusuke