Other Parts Discussed in Thread: UCC21750
Hi all,
Wanted to use AIN in UCC21750 for measuring Vdc = 1000V, but i have some doubts regarding duty variation over temperature. In datasheet it is mentioned that duty may vary 15% Vin = 4.5V , in SLUA988 it is shown that absolue error with Ain is 5% accuracy and after calibration we can achieve +/-1%. Is the duty error a constant or it varies with temperature. If it is constant then we may calibrate it at single point of T=25 deg