This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54917: TPS54917 Low side mosfer Negative Spike

Part Number: TPS54917


Hi SIR

We use tps54917 to design 3.3V to 1.0V_9A power supply for asic use.

A phenomenon was found during the measurement.

As long as the inductor current enters the continuous conduction mode (about 1A),

Low Side Mosfet_Vds shows obvious negative  spike and exceeds the maximum absolute value of the specification.

How can we improve this phenomenon?