Hello,
In the datasheet of TPS2663 the Input and output of the IC goes through pin no. 1 ,2 and 17,18 respectively. But the reference layout file of TI shows the connections of Input and Output through pin no. 1,2,24 and 17,18,19 respectively whereas in the datasheet PIN 19 and Pin 24 is no connection PIN.
Can you please confirm on the above discrepancy whether to use both the NC pins for Input and Output connections?