This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54260: Output is unstable under -35 temperature degree

Part Number: TPS54260

Dears,

We found if some TPS54260 can't work under -35°C. If we test ABA, replaced TPS54260 can work.

I get a pic TPS54260 can't work status as below.

Blue line is voltage output pin's fig under -35°C. It should be 12v if work normal.

If we change test temperature to -25°C, it will work normal.

So how can deal this issues. Thanks.