Part Number: BQ27750
Hello,
in our device we're using a LiPo battery pack with BQ27750 fuelgauge chip.
We want to use the remaining energy in cWh and a constant power consumption value to calculate and display the remaining runtime of our device.
In several logs of discharging our device we were facing a non-linearity of the remaining energy value after about 100 minutes of device runtime.
Attached you will find a typical log file where you can see in column "Z" the remaining energy in cWh which is descending from line to line in a linear way.
In line 83 you can see that the remaining energy value jumps from 558 to 570 cWh without any change of the load.
This behavior is the same in all log files and for different battery packs + devices and leads to an increase of remaining runtime of about 15 minutes which will be displayed during discharge process.
We want to understand why the the remaining energy is jumping all the time after more or less the same device runtime (after about 100 minutes) and if there is a way to prevent this jumps.
Thanks in advance!
Best regards,
Marcel