In our application we use a Hercules RM48x MCU paired with the TPS65381A-Q1.
Unfortunately we loaded the MCU with firmware that does not handle the setup of the TPS65381A-Q1 correctly.
We are now stuck in a loop where the TPS endlessly resets the RM48, preventing us to load a correct firmware onto the RM48.
Is there anyway without physically affecting the nPORST line to end this reset loop and reprogram the RM48?