Can this charger be used to charge 24V battery packs ?, looks like the input power source can go up to 30V, but smbus commands are only up to 19V. Is there a safe way to modify voltage feedback and shift the charger range higher then 19V?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can this charger be used to charge 24V battery packs ?, looks like the input power source can go up to 30V, but smbus commands are only up to 19V. Is there a safe way to modify voltage feedback and shift the charger range higher then 19V?
The maximum recommended input voltage is 24V. So, please keep the input voltage lower than that. 19V output is good for a notebook application.
If you have another applicaion, we have higher ouput voltage charger, such as bq246xx. What are the input and output voltage range?
Unfortunately non of them has SMbus logic built in, so I can not use them. I will have to make my own
Thanks,
I am not sure how do you build your board? But, there is a high voltage charger post. http://e2e.ti.com/support/power_management/battery_management/f/179/p/88984/307999.aspx#307999
Also, another idea is:
Convert InputCurrent(); chargeCurrent() and ChaargeVoltage() command to analog signals to setup bq24610 's ACSET; ISET1 and VFB resistor divider.