Q1 Is the SOC gap appropriate? It seems that there is a large gap.(20% point)
a)Full Charge
b)Discharge to target point by using passed charge.
c)Rest 10min
d)Remove and insert battery, then check the SOC.
※gauge/charge IC is in system side.
d)Repeat b)~d)
follow is the result.
SOC check points Calculate SOC
100% 99%
90% 89%
80% 79%
70% 69%
60% 59%
50% 48%
40% 37%
30% 27%
20% 14%
10% 8%
5% 4%
※room temperature
※learning cycle completed
Q2 Should Qmax delta and Ramax delta be large when conducting a learning cycle?
If default,is Ra table used in Q1 incorrect?