Hey,
I was using LMG1210 in independent input mode (IIM). I'd like to confirm if LMG1210 would work for negative rail voltages on HB & HS? According to the datasheet, it should be able to switch as long as HB-HS < 5.5 V. However, I'd like to confirm it before incorporating it in my application. I am attaching a snippet of the circuit. I will only be using the high side without bootstrapping. Any help is appreciated.
Thanks,
Karan