Hi team,
What should we consider when we use this device with -30℃ to 100℃?
Which parameter will change and what will occur for that?
Regards,
Ochi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
What should we consider when we use this device with -30℃ to 100℃?
Which parameter will change and what will occur for that?
Regards,
Ochi
Hi
Because it's a qualified device so we can ensure the device feature within the temp spec in datasheet.
I think "-30℃ to 100℃" means ambient temp, the key point for customer is to consider the consumption of device.
You should make sure the device work in the condition that the junction temp is below 150 ℃.