This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5022: Reference design ASAP

Part Number: LM5022
Other Parts Discussed in Thread: LM51551

I am looking ASAP for a reference design of isolated DC/DC 5V input, 3.3V with 2.5A output.

Readily made bricks I found in this range, are ridiculous expensive (>20$) so we are trying to settle a design for our future product.

The most closest reference design will be this one, using LM5022, but the problem is that minimum input is 6V and we need 5V

http://www.ti.com/tool/PMP9282 

The big question is: can we replace the buck with one that accepts 5V on input?

Thanks in advance.

  • Hi,

    You can design a flyback converter which allows you to do a step-down operation to what you need. If you cannot use the LM5022 because of the minimum input range, I would recommend using the LM51551 (since you will need hiccup-mode) in a flyback converter. It's minimum operating range is 3.5V, which is within your limitations.

    Datasheet is attached: http://www.ti.com/lit/ds/symlink/lm5155-q1.pdf

    Please see the design guide if necessary: ti.com/lit/an/snva866/snva866.pdf 

    With the LM51551, it looks like the power-stage should be quite similiar to the current design in PMP9282. Please let me know if you have any questions. 

    Thanks,

    Richard

  • Hi Richard,

    Thank you so much, this is exactly what we need (perhaps not 4A)!

    Now in snva866.pdf the transformer part number is wrong, I cannot find at Wurth this, nor at Digikey or others.

    What do you think, this one is a good replacement?

    PA3855.004NL  (9..38V input + 10V aux, 2x3.3V output)

    productfinder.pulseeng.com/.../P719.pdf

    Thank you! 

  • Hi,

    You should be able to use the transformer, but I would make sure that at a lower input voltage, your ripple current is not high enough to saturate the transformer. To be safe, I would recommend talking to the transformer vendor to double check and see if they have better solutions. 

    Thanks,

    Richard