This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61169: About efficiency@24V output

Part Number: TPS61169

Hello,

 Regarding to efficiency on TPS61169, my customer is asking a question.

Their conditions are following.

Vin 3.0V

Vo typ 24V(21.7~25.6V)

Io  80mA

(Question)

In above case, what is the efficiency under these conditions?

I estimate it will be less than about 85% from datasheet figure 8/9.

 

Regards,

Tao_2199