Hello,
Regarding to efficiency on TPS61165, my customer is asking a question.
Their conditions are following.
Vin 3.0V
Vo typ 24V(21.7~25.6V)
Io 80mA
(Question)
In above case, what is the efficiency under these conditions?
I estimate it will be less than about 89% from datasheet figure 2
Regards,
Tao_2199