This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25713: 1 cell buck charger with boost operation

Part Number: BQ25713
Other Parts Discussed in Thread: BQ24800

We are looking for Li-ion 1 cell buck charger with boost operation.

Vin: USB 5V
VCHG: programable, typ 4.2V
ICHG: up to about 5A

Boost operation: 12Vout, 2.3A from battery power

I think bq25713 can meet these requirement, is this right? Please let me know if you have any other devices.

If bq25713 is best device, can we use bq25713 with 2 switch circuit?
In this use case, bq27513 is used only as buck charger and boost converter. So I think Q3 and Q4 is not needed.

Best Regards,
Kohei Sasaki