Other Parts Discussed in Thread: TPS92691, TPS92691EVM-752
I trying to change TPS92691EVM-001(SEPIC) to wide voltage range Boost LED driver with low-side sensing.
Please let me know about external compensation parts;
①Can boost LED driver apply to use integral compensation? (Datasheet equation (37))
②If ① is yes, which ωp equation for buck or boost by table-1(Datasheet P24)?
Or, please let me know equation for Boost LED driver's Ccomp/
③ Ccomp changed 20nF to 220nF ⇒ normal operation range was expand
Ccomp changed 220nF to 1μF ⇒ specification was not improvement
I guess that above reason (220nF to 1μF) is limit to TPS92691 internal transient, correct?
【Background】
・Vin: 24V ⇒ Vout: 36V~110V, Iout: trying to reach 500mA_max
(External parts were changed match high voltage specification, etc)
・At first based on proportional integral compensation circuit (equation (38)~(40)), waveform was oscillation.
・When changed integral compensation, to certain extent was normal operation.
When above the certain Vout or Iout (or Pout?) level, it occur oscillation.
Best regards,
Satoshi