Other Parts Discussed in Thread: UCC5350
Hi Team,
I am posting this on behalf of the customer and I use UCC27282 as TI part because of I that this is the nearest possible product I found so far but I hope someone can recommend a better TI part if we have this:
The customer is looking for a gate driver, high side to low side (instead of low- to high-side). The input of the gate-driver is referenced to 150 VDC, the output is referenced to 0V.
Other information I got from the customer:
"The topology is an LLC-converter for railway-application and it's going to be used on various projects.
For a high power application, we want to implement a LLC full-bridge on the primary-side (normally only half-bridge). Therefore, the high-side driver of the LLC-controller has to drive a high-side FET (directly with LLC-controller integrated high-side gate driver) AND a low side FET at the same time. To drive the low-side FET with the same timing as the high-side FET, we need a high-to-low-side gate driver. The input-voltage of the LLC-converter is 110 - 150 VDC, therefore, the high side driver of the LLC-controller is referenced to this voltage, while the low-side FET is referenced to 0 VDC."
Here's the customer circuit diagram.
Please let me know if you need more information.
Thanks!
Jonathan