This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/TLV61046A: Design Cannot be Created - Inputs seem reasonable.

Part Number: TLV61046A
Other Parts Discussed in Thread: TLV61048

Tool/software: WEBENCH® Design Tools

Hi,

I wish to use WebBench with TLV61046A to check a design I have. Basically the design works, but I'm experiencing some thermal issues.

My inputs into web bench are:

Vin = 4.0V - 5.5V

Vout = 12V

Iout = 0.3A

Temp = 30C

All of these parameters should be within the devices capabilities (i.e. load switch max = 0.68A) but WebBench says the device does not work with those inputs.

Would anyone be kind enough to confirm?

Thanks

Stomp!