Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS546C23EVM1-746: Not receiving ACK through PMBUS from either of the devices

Part Number: TPS546C23EVM1-746
Other Parts Discussed in Thread: TPS546C23

Problem :

I am not receiving ACK through PMBUS from either of the devices addressed 27 and 36 (in decimal). I have an FPGA trying to emulate the master. 

Setup :

I have pulled up Clock, Data lines (9,10 pins of PMBUS) to 3.3 V with 1Kohm resistors. DIOs from the FPGA are given to the Clock and Data lines with common ground(pin 6). I have verified the address byte using the DSO. I start the PMBUS command then I send the address byte (0011011 0 - along with 0 for write operation), I am not receiving ACK from the device (both 27d or 36d). I have powered the device with 6.5 V supply.

Please let me know if I am missing something and let me know the steps to debug the circuit.

Thanks in advance

Rahul