Hi,
I have an LM5116 with the switching frequency set to 260KHz. 48V input and 12V output. Under 2A load, I can see that the switching frequency varies between 260Khz, 130KHz and 86.6KHz which is half and one third of the set switching frequency. Under higher loads, I can see that the switching frequency is mostly 260KHz. Is this expected behavior or is there a problem with my compensation network/ramp?
Thanks