Other Parts Discussed in Thread: LM3406HV, LM3402HV, TPS92692, TINA-TI
Hi All,
I am looking for a led driver for a motorbike headlight.
It should be a buck that can withstand an input voltage of at least 75V.
The characteristics of the circuit in which we would like to implement the LED driver, in its normal operation, are:
• Vin between 18V and 32V;
• as load only one branch including 3 LEDs in series, whose total drop is about 9V +-1V);
• the load current must be 200 mA;
• there is no need for dimming.
I found the component: LM3406HV-Q1.
But I noticed that on page 6 of the datasheet there is the load efficiency / current graph, and the behavior for a 200 mA load is not shown.
So, could this device fit for a load current of 200 mA or is it too low?
Would you have other devices to recommend to me for the application I described to you?
Important are the dimensions as small as possible, and that has the minimum necessary to allow the piloting of the LEDs when powered,
An interesting feature would be the possibility of having the spread spectrum, in order to reduce emissions.
Many Thanks,
Antonio