This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

REF3025: Reverse current on output for REF30XX

Part Number: REF3025

Hi Team,

REF3025 and REF3033 was used in customer's project.There is a problem when REF30XX is used for offset voltage.

Here is the schematic on customer site:

When Vin is less than 2.5V, REF3025 output a current, it's OK;

When Vin is bigger than 2.5V(Sometimes 5~7V), the current flow to REF3025. Is it OK for REF30525? How much current can REF3025 hold in this application?

BR

Songzhen Guo