Hello,
Could someone provide a bit more guidance on the protection circuit mentioned in section 8.1.1.7 of the LM3410 datasheet?
My LED string has Vf=8-9V and we'll be driving it with 500mA normally. I calculate R(fb) = 390mOhm for the normal case.
If I use a 10V zener for D2 in Figure 14, it will never fire under normal circumstances. Then R3+R1 will drop the 10V (assuming high-impedance into VFB pin of LM3410). It we cap at 500mA then R3 must be ~19.6ohms. That is OK, but that resistor will be dissipating 4.9W! I don't see any way around that. Any ideas without adding some significant circuitry (opamps, etc)?
James.