Tool/software: WEBENCH® Design Tools
Hi,
I use the Webench Power Designer to develop a boost converter using TLV61046A.
The Boost circuit will converte 5Vcc to 24Vcc@60mA.
The circuit works but a load at 4mA (the minimum load) the voltage of the output of the converter is 13V.
I don't know what hapens and the components are the same as the bill of the material.
Could help me with this circuit or I need to change to get 24V@60mA output?
Thank you.
Edso