Other Parts Discussed in Thread: TL5001, TL1451, TL1451A
The thermal rating for the TL1454A appears to be -20°C to +85°C as shown in the absolute maximum ratings. I am curious what parameters or degradation happen if the device is operated over the industrial -40°C to +125°C range?
It appears to me per the graphs that the SCP pin UVLO could be most affected as would the Error amplifier voltage swing and possibly the output push-pull transistor voltage drop?