This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5021: Soldering specification

Part Number: LM5021


Hi Team,

Is there a recommended soldering equipment specification can refer to?
In addition, is there an limitation for the temperature and operating time that can be provided? Will there be a risk of damage if the temperature is exceeded?

Thanks and best regards,

Jamie

  • Hi Jamie, I will reply to you tomorrow. —— Teng

  • Hi Jamie,

    Reflow profiles are dependent on numerous factors including package type, number of components, board layers, board size, reflow oven accuracy and process and more.

    Because of the number of variables it is not possible to provide a single reflow profile that is representative of every board using a specific package type. Typically manufacturing houses have reflow profiles in place and modify them for specific hardware.

    For optimal reflow results in achieving consistent solder joint geometries the reflow profile should be developed in cooperation with the solder paste supplier and with the equipment supplier as needed. The solder paste vendor's datasheet includes recommendation for reflow profiles based on alloy melting temperatures and flux activity. These recommendations must be followed to achieve optimal flux activity resulting in wetting of the lead surface. The flux activity in the solder paste plays an important role in facilitating solder wetting resulting in consistent solder joint geometries.

    These documents details some of the issues involved here, I believe they will answer most questions:

    http://www.ti.com/lit/an/spraby1a/spraby1a.pdf

    http://www.ti.com/lit/pdf/SNOA550                Handling & Process Recommendations

    http://www.ti.com/lit/pdf/SNOA549                Absolute Maximum Ratings for Soldering 

    http://www.ti.com/lit/an/slua271b/slua271b.pdf

    http://www.ti.com/lit/an/slta054a/slta054a.pdf                                     

    Regards,

    Teng