Hi
The specification of TPS659039 mentions:
SMPS4 and SMPS5 cannot be used as separate converters. In dual-phase configuration the two interleaved synchronous buck regulator phases with built-in current sharing operate in opposite phase.
SMPS4 and SMPS5 of TPS659039 chip designed on DEMO board are used together.Can supply 4000mA of current .
But the load of our circuit only needs less than 2000mA of current, so only one SMPS4 or SMPS5 is needed. We tried to open SMPS5 and only keep SMPS4. The circuit can operate normally. I want to know can I keep SMPS5 open? What are the hidden dangers? For example in RE