Other Parts Discussed in Thread: LM5122
Tool/software: WEBENCH® Design Tools
Hi,
LM5122ZA Feature shows frequency up to 1 MHz, why I cant simulate over 352.94 1KHz?
So I setting Rt as 18 KOhm, the frequency is 500 KHz, but it shows an alert
M1 Tj:341.27 °C Specification: <150.00 °C
M1 MOSFET junction temperature is too high
-
Decrease Switching Frequency to decrease MOSFET or Diode switching losses
-
Decrease ambient temperature
-
Decrease thermal resistance by adding a heat sink if feasible
-
Increase the copper area and thickness of the board
I'd change many MOSFET with low Ciss/Coss, low Qrr.
It still shows this alert. I have size issue, can't design the frequency under 500 KHz.
Here is my setting specification as below:
Vin=19V, Vout=60V, Iout=1.6A (Pin = 100W)
Frequency = 500 to 800 KHz
One more question about current limit
I want set Ipeak=7A, according to section 7.3.10, Rs=10 mOhm
According to section 8.1.4, if I want to use Rdcr of inductor, how to calculating 7A limit?