Other Parts Discussed in Thread: TPS61099
Hi
I want to use the booster for a USB OTG device, to provide 5V to VBUS from a Lion battery.
I also will be using the same VBUS rail for charging the battery. I was planning on a circuit along the lines of what is shown in figure 37, with a switch on the input to the inductor, but will I also need a switch on the output or can the IC handle 5V on the output with the input disconnected?
Thanks