Question: I am using CSD19534Q5A MOSFET for the power supply section of automotive electronics. Can I get the confirmation from the TI that the Fit rates and MTBF data (1.7PPM and 603 Million operational hours @ 125°C) associated with the above-mentioned part are validated if used in automotive applications within the specified thermal and electrical characteristics by the datasheet? Also, is there any alternate of CSD19534Q5A which is AEC-Q qualified with the same specifications and footprint?