Other Parts Discussed in Thread: , BQ25895
Q1. I've looked all over and can't find what REGN and PMID stand for.
Q2. In section 5 of the datasheet (SLUSB97A) the last sentence of the 4th paragraph states"When the full battery falls below the recharge threshold, the charger will automatically start another charging cycle." and in section 8.3.3.1 the last sentence of the paragraph under the bullets states "When a full battery voltage is discharged below recharge threshold (REG04[0]), the bq24195L, bq24195 automatically starts another charging cycle." The Battery Recharge Threshold (VRECHG) can be set to 100 or 300 mV with the default being 100 mV. What is the 100 or 300 mV referenced to? It can't be referenced to ground or the recharge cycle wouldn't start until way below 3.0 V. I'm using a LiCoO2, 2000 mAh, 3.7 V battery.
Thanks Much!