Other Parts Discussed in Thread: BQSTUDIO, BQ76940, TIDA-00792, BQ78350, EV2400
Using the BQStudio software the bq78350-R1 shows up at launch, but only appears for a few seconds. When trying to change the settings an error code pops up that says, "operation failed because initial read of all data flash failed." What does this mean and do I need to configure this device in order for it to communicate with the BQStudio? I assumed this would auto detect the configuration. For reference I am using 11 18650s for this device.