I use TLV70033DDCR.
I explain usage.
I connect 5V to the input pin and connect a 1uF ceramic capacitor to the output pin.
I have not connected the load.
When 5V is turned on, the voltage gradually increases.
When it reaches about 2V, the output of TLV70033 DCR rises suddenly and follows the 5V voltage from there.
Why is the output not linear?
I don't know why he got up suddenly.
Please kindly advise.